AXIS#.UNIT.POUT

Description

AXIS#.UNIT.POUT is used with AXIS#.UNIT.PIN to set application specific units in AXIS#.UNIT.POUT. This parameter is used as follows in the drive unit conversion:

  • For position, this parameter sets the units as Custom Units/revolution.
  • For velocity, this parameter sets the units as Custom Units/second.
  • For acceleration/deceleration, this parameter sets the units as Custom Units/second2.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

User units.

Range

1 to 4,294,967,295

Default Value

20

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.UNIT.POUT

5010h

02h

Unsigned32

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6604

1

6604 (0x19cc)

AXIS1.UNIT.POUT

Unsigned32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.UNIT.POUT

6604

Unsigned32

Read/Write

-